AXIS#.MOTOR.SERIALNUM

This parameter is the motor serial number.

 

Context

For more information see Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

 

General Information

Type

Read

Units

N/A

Range

14chars

Default Value

empty

Data Type

String

See Also

N/A

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.MOTOR.SERIALNUM

500bh

2ch

String(15)

-

-

Read only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6242

1

6242 (0x1862)

AXIS1.MOTOR.SERIALNUM

String

Read Only

No

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.MOTOR.SERIALNUM

6242

String

Read Only

-